;PlatformIO User notes:

;It is possible to load settings from the calling program rather than modifying
;the library for each project by modifying the "platformio.ini" file.

;The User_Setup_Select.h file will not load the user setting header files if
;USER_SETUP_LOADED is defined.

;Instead of using #define, use the -D prefix, for example:

; PlatformIO Project Configuration File
;
;   Build options: build flags, source filter
;   Upload options: custom upload port, speed and extra flags
;   Library options: dependencies, extra library storages
;   Advanced options: extra scripting
;
; Please visit documentation for the other options and examples
; https://docs.platformio.org/page/projectconf.html

[env:esp32dev]
platform = https://github.com/platformio/platform-espressif32.git#feature/arduino-upstream
board = esp32dev
framework = arduino
lib_deps = bodmer/TFT_eSPI@^2.4.31

build_flags =
  -Os
  -DCORE_DEBUG_LEVEL=ARDUHAL_LOG_LEVEL_DEBUG
  -DUSER_SETUP_LOADED=1
  
  ; Define the TFT driver, pins etc. here:
  -DST7789_DRIVER=1
  -DTFT_WIDTH=128
  -DTFT_HEIGHT=160
  -DTFT_MISO=19
  -DTFT_MOSI=23
  -DTFT_SCLK=18
  -DTFT_CS=5
  -DTFT_DC=19
  -DTFT_RST=4
  ;-DTFT_BL=21
  ;-DTOUCH_CS=22
  -DLOAD_GLCD=1
  -DLOAD_FONT2=1
  -DLOAD_FONT4=1
  -DLOAD_FONT6=1
  -DLOAD_FONT7=1
  -DLOAD_FONT8=1
  -DLOAD_GFXFF=1
  -DSMOOTH_FONT=1
  -DSPI_FREQUENCY=27000000